09/15/2014Delta Unveils the World's First Ultra-bright Laser-based Video Wall at InfoComm India 2014
Mumbai, India, September 15, 2014 – Delta, a global leader in thermal and power management and pioneer in display solutions, announced today it will unveil the world's first ultra-bright Laser-based Digital Light Processing (DLP®) video wall at InfoComm India 2014. Delta's laser-based DLP® video walls feature industry-leading performance with brightness of up to 1,800 lumens and significantly improved energy savings of up to 10%. Through the integration of Delta's advanced control systems, –DVCS and MiNiCON– our video walls become total solutions for applications demanding 24/7 operations. A platinum sponsor for the event, Delta offers visitors live demonstrations of its innovative display and monitoring solutions, all of which are designed to maximize reliability and productivity for control room, public display and visualization applications. Compared to similar LED-based DLP® video walls, Delta's laser version boasts an array of benefits, including better performance via incredible brightness of up to 1,800 lumens and a high contrast ratio of up to 2000:1. In addition, the redundant light source and power supply in the new Laser-based DLP® video wall guarantee no downtime, making it ideal for applications demanding 24/7 operations while enhancing energy savings by up to 10% (versus traditional cubes), thus, providing a remarkable reduction in costs of ownership. State-of-the-art projectors from Vivitek, a brand for Delta, will also be part of our showcase at InfoComm India 2014 and will offer highly advanced and versatile display technologies such as edge-blending imaging and 3D solutions especially for large venue applications. In addition, Delta will offer a sneak preview of its ultra-narrow bezel LED LCD video walls, featuring the slimmest bezel in the market. These video walls allow a seamless connection between each display to create a powerful, high-impact visual experience for viewers. With Ultra narrow bezel LCD Video wall, Delta will exhibit one of the world's most advanced display control system: The Distributive Vision Control System (DVCS). Through the integration of Delta's DVCS, our video walls become total solutions for applications demanding 24/7 operations. Delta would also be showcasing its industry-first Ultra Slim Cube Series featuring super-efficient LED light engines, redundant power supplies, auto alignment, and auto color calibration used in mission-critical, control room and broadcast applications. Bright, high impact Indoor LED displays and LCD Monitors will be showcased at the front of the Delta booth which will bring visual excitement to both indoor and outdoor environments. Delta will exhibit its state-of-the-art display & monitoring solutions during InfoComm India 2014 at booth E1, Bombay Exhibition Centre, Mumbai, India from September 17th to 19th. InfoComm is a leading and the most prestigious audio visual Expo designed for professionals in the audiovisual, information communications and systems integration industries.